Running sample VoIP application on Linux SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running sample VoIP application on Linux SDK

2,137 Views
lyfsci
Contributor III

Hi Experts,

Is there any demo application or package to run the sample VoIP application along with SIP to run using the IMX6 SL EVM board ?

Kindly provide some info on this  ?

Regards, Lyf

Labels (3)
1 Reply

1,802 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

seems there are no free i.MX6 VoIP stacks, one can look

at partners demo

i.MX6 Android KitKat Enterprise VoIP Handheld P... | Freescale Community

or consider ls1021  (ARM A7 core) VoIP

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/LS1021A_IOT_GTW_RN.txt

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------