Run the program after jumping to SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run the program after jumping to SDRAM

833件の閲覧回数
stanley-kylee
Contributor II

Hello.

 

Currently, RT1020-EVK is running based on XIP.

After every boot, I want to move the code from serial flash to SDRAM and then jump to the first point in SDRAM. (the program start point).

During operation with XIP, it is necessary to erase and write serial flash, but the erase operation takes too long.
There is a way to run it from SDRAM from scratch without using XIP, but the procedure to download the program is very complicated. (Not suitable for mass production)
So I try to jump after copying the program to SDRAM.

Anyway, after booting, I want to copy the first 2MByte area of serial flash to SDRAM and jump to the starting point of SDRAM.

Please check if what I did is correct.
(Probably there is a missing process.)

-----------------------------------

1. SEMC initialization

2. Copy serial flash data to SDRAM
    → Source(Serial Flash) : 0x60000000U ~ (0x60000000U + 2MByte)
    → Destination(SDRAM) : 0x80000000U ~ (0x80000000U + 2MByte)

3. Jump to SDRAM

-----------------------------------

When running after jumping to SDRAM in the same way as above, are there any more settings that need to be changed?

I attach the project file.
(source/semc_sdram.c)

Thanks in advance for your reply.

 

 

 

0 件の賞賛
返信
0 返答(返信)