Run application using OCRAM in imx6dl sabresd reference board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run application using OCRAM in imx6dl sabresd reference board

1,110件の閲覧回数
winstonjacob
Contributor IV

I am using imx6dl sabresd reference board, and I want to run a sample application using OCRAM, and I referred the link mentioned below.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iRAM-OCRAM-i-MX6-SDK-Application/ta-p/11...

I compiled the imx6 sdk  and I got iram.bin and iram.elf, then flashed the u-boot image as well as iram.bin to sdcard, then I booted the board, and I executed the command in u-boot prompt, and I mentioned the log here, please verify and help me to run the application in OCRAM memory.

 

U-Boot 2017.03 (Feb 14 2019 - 15:48:31 +0530)

CPU: Freescale i.MX6DL rev1.1 996 MHz (running at 792 MHz)
CPU: Commercial temperature grade (0C to 95C) at 31C
Reset cause: POR
Model: Freescale i.MX6 DualLite SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net:
Warning: ethernet@02188000 using MAC address from ROM
eth0: ethernet@02188000 [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
=> bootelf 0x10800000
## No elf image at address 0x10800000
=> mmc dev 1
switch to partitions #0, OK
mmc1 is current device
=> mmc read 0x10800000 0x800 512

MMC read: dev # 1, block # 2048, count 1298 ... 1298 blocks read: OK
=> bootelf 0x10800000
## No elf image at address 0x10800000

 

Regards

Winston

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,106件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Winston

 

in general one can try to load bin file using mfg tool as described on

https://community.nxp.com/t5/i-MX-Processors/Loading-Sample-SDK-on-IMX6-SABRE-board/m-p/320466

change ucl2.xml :

"SabreSD-SD" profile:

<LIST name="SabreSD-SD" desc="USB SDP">
<CMD state="BootStrap" type="boot" body="BootStrap" file ="test.bin" >Loading image</CMD>
<CMD state="BootStrap" type="jump" > Jumping to image. </CMD>
<CMD state="Updater" type="push" body="$ echo Load Complete!">Done</CMD>
</LIST>

Mfg tool can be found on

https://www.nxp.com/design/software/embedded-software/i-mx-software:IMX-SW

 

Best regards
igor

0 件の賞賛
返信

1,084件の閲覧回数
winstonjacob
Contributor IV

Thanks for your immediate reply @igorpadykov ,

       Using mfgtool I can able to load the sample application which NXP provided (RVDS 3.1 MX6DQ_SDP_LED.ZIP.zip) , but in this sample app I have to do some modification and I have to cross compile and execute,

RVDS 3.1 MX6DQ_SDP_LED.ZIP/MX6DQ_SDP_LED$ arm-linux-gnueabihf-gcc main.c -o led.bin

      If I cross compile using the above command, I am able to generate a bin file, but that bin file I am not able to load via mfgtool, while loading mfgtool throwing error. Can you please give me the compiling steps for RVDS 3.1 MX6DQ_SDP_LED.ZIP.zip application.

 

REF LINK

=======

https://community.nxp.com/t5/i-MX-Processors/Loading-Sample-SDK-on-IMX6-SABRE-board/m-p/320466

Regards

Winston

 

 

 

0 件の賞賛
返信