Run NXP AOSP image on Android Emulator based on x64 host machine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run NXP AOSP image on Android Emulator based on x64 host machine

2,438件の閲覧回数
arpandutta0000
Contributor I

Hi,
I am trying to run the NXP AOSP image (Android 12.1.0_1.0.0 (L5.15.52_2.1.0 BSP) i.MX 8M Plus EVK)​​​ on android emulator as currently the 8MPLUSLPD4-PEVK board is not available due to logistic reasons.

The NXP AOSP image is based on ARM from what I understand, but I want to run it on emulator on my local Ubuntu system which is based on x64 architecture. While booting up the android automotive emulator with the above mentioned NXP image, I am getting this issue:
error: AVD's configuration is missing a kernel file

Is it possible to run NXP AOSP image on a x64 based android automotive emulator?

タグ(2)
0 件の賞賛
返信
1 返信

2,404件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Do you mean these images https://www.nxp.com/design/software/embedded-software/i-mx-software/android-automotive-os-for-i-mx-a...

These are only for the i.MX8QM and i.MX8QXP.

0 件の賞賛
返信