Run MCU from NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run MCU from NAND

1,118件の閲覧回数
TM_MI
Contributor III

Hello,

Is it possible to flash the blinky SDK on a the raw NAND flash memory using Jtag and MCUxpresso.

I know that the configurations has to be changed to serial downloader but I think I have to use a bootloader like Ozone Segger.

Processor used is RT1170.

Thank you,

Tarek

0 件の賞賛
返信
1 返信

1,109件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @TM_MI ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to flash the blinky SDK on a the raw NAND flash memory using Jtag and MCUxpresso.
-- No, I'm afraid not.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信