Rpmsg enabling patch file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rpmsg enabling patch file

ソリューションへジャンプ
3,481件の閲覧回数
arunsathian
Contributor III

Hi,

Is the attached patch file suitable for L5.10 also? 

or else what are the changes need to be done in this patch file.

0 件の賞賛
返信
1 解決策
3,382件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @arunsathian 

You can refer  AN5317 Loading Code on Cortex-M from U-Boot/Linux for the i.MX Asymmetric Multi-Processing Application Processors 

https://www.nxp.com/docs/en/application-note/AN5317.pdf

 

Best Regards

Zhiming

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,471件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @arunsathian 

You can't use it directly, there are lots of changes in framework and dts.

 

3,464件の閲覧回数
arunsathian
Contributor III
Hi @Zhiming_Liu
what are the changes need to be done in this patch file?Can you please explain in a brief?
0 件の賞賛
返信
3,457件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The device tree changes a lot(arch/arm64/boot/dts/freescale/imx8qxp-mek-rpmsg.dts), and L5.10 don't use rpmsg driver anymore, it uses remoteproc framework.

3,408件の閲覧回数
arunsathian
Contributor III
Hi @Zhiming_Liu
Are you saying that for L5.10 version we strictly need to use remoteproc instead of rpmsg?
If do so can you please share any documents related with it.
0 件の賞賛
返信
3,383件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @arunsathian 

You can refer  AN5317 Loading Code on Cortex-M from U-Boot/Linux for the i.MX Asymmetric Multi-Processing Application Processors 

https://www.nxp.com/docs/en/application-note/AN5317.pdf

 

Best Regards

Zhiming

0 件の賞賛
返信