Rotate Image Using i.MX6 VPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Rotate Image Using i.MX6 VPU

3,235 次查看
cigdemyavuzcayc
Contributor I

Hi,
We are taking 720x1280 or 1080x1920 input image from our camera. After encode the image we want output resolution to be 1280x720 or 1920x1080. Is there any restriction in resolution when we rotate the input image 90 or 270 degree using i.MX6 VPU?

Kind regards,

Cigdem

标签 (1)
0 项奖励
回复
5 回复数

3,081 次查看
cigdemyavuzcayc
Contributor I

As we want to record encoded file and will display it on another media, I need to rotate before encode. From "i.MX VPU Application Programming Interface Linux® Reference Manual " Rev. 0, 03/2016 Section 4.4.2.2, I understand that it is possible to rotate using VPU. I can rotate images 90 or 270 degree with resolution up to 720x720 without any problem. I am getting error for 720p and 1080p. Does VPU support 90 degree rotation for these resolutions?

Kind regards,

Çiğdem

0 项奖励
回复

3,081 次查看
joanxie
NXP TechSupport
NXP TechSupport

how did you rotate by vpu with 720P? could you give me your test steps? and what error you get? first, vpu get video from IPU which has IC hardware module can support rotate, I don't know what your operation, maybe you can share it

0 项奖励
回复

3,081 次查看
cigdemyavuzcayc
Contributor I

Yes, I'm talking about i.MX6DL sabre board.

0 项奖励
回复

3,081 次查看
joanxie
NXP TechSupport
NXP TechSupport

one can try to use IPU or GPU to rotate

0 项奖励
回复

3,081 次查看
joanxie
NXP TechSupport
NXP TechSupport

vpu does't support rotate, if you need to rotate, IPU or GPU do this job, what board are you talkinig about? imx6dl board?

0 项奖励
回复