Rootfs for QEMU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,100件の閲覧回数
alexishernandez
Contributor III

Hello everyone,

Is there any way to get the root file-system from an image deployed with bitbake?, so i can use it with QEMU and emulate an i.mx6 processor.

I want to use the runqemu-extract-sdk <core-image-sdk-imx6ulevk-xx.tar.bz2> MY_IMX6ULEVK_ROOTFS
Best regards.

ラベル(4)
0 件の賞賛
返信
1 解決策
2,581件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Alexis,

unfortunately qemu is not supported for i.MX platforms. However you may look at the following

 

IMX7 Hypervisor mode


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,582件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Alexis,

unfortunately qemu is not supported for i.MX platforms. However you may look at the following

 

IMX7 Hypervisor mode


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,581件の閲覧回数
alexishernandez
Contributor III

Thanks Carlos

0 件の賞賛
返信