Reuse CAN interface for UART communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reuse CAN interface for UART communication

1,049 Views
shailendrakarod
Contributor I

Is there a way to re-purpose the two CAN (DB-9) interfaces on i.mx 6solox dev board for UART communication?

Labels (1)
0 Kudos
Reply
1 Reply

990 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shailendra

muxing options are given in Table 4-1. Pin Assignments i.MX6SX Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

and seems there are no options for uarts.

Schematics (1)
IMX6SOLOX-SABRESDB-DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply