Return mode on iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,338件の閲覧回数
AlbertT
Contributor V

Hello !

I was wondering what exactly is the return mode which is present on the iMX6 ? I think it's also called FSL mode, the reference manual mention it but doesn't really describe what it is and what we can do with it. It seems to be something between open and closed mode.

Regards,

Jocelyn Kevorkian

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
4,781件の閲覧回数
Yuri
NXP Employee
NXP Employee

The FIELD RETURN mode is described in the i.MX6 Security Reference Manual.

元の投稿で解決策を見る

8 返答(返信)
4,782件の閲覧回数
Yuri
NXP Employee
NXP Employee

The FIELD RETURN mode is described in the i.MX6 Security Reference Manual.

4,781件の閲覧回数
AlbertT
Contributor V

Yep I found it after !

0 件の賞賛
返信
4,781件の閲覧回数
AlbertT
Contributor V

Well, ok then.

Thanks.

0 件の賞賛
返信
4,781件の閲覧回数
Yuri
NXP Employee
NXP Employee

In the field return mode Security configuration - is as Open, also FSL Test modes are re-enabled
to allow device testing.

4,781件の閲覧回数
AlbertT
Contributor V

Hello Yuri,

Ok thanks ! Is there a document where I can find more details about FSL tests modes ?

0 件の賞賛
返信
4,781件の閲覧回数
Yuri
NXP Employee
NXP Employee

Alas, I never seen FSL tests description.  

0 件の賞賛
返信
4,781件の閲覧回数
AlbertT
Contributor V

Hello Fabio,

On page 454 of the RM, we have the description of boot security settings, there are open/closed/field return which is described by "This level is intended for parts returned from shipped products".

On page 456, an eFuse is called FIELD_RETURN and its definition is "Enables FSL reserved modes".

So I would like to know what is field return, and how we can use it ?
Thanks !

Jocelyn Kevorkian

0 件の賞賛
返信
4,781件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Can you provide more context to your question? I am not able to understand what you are asking with your current description.

0 件の賞賛
返信