i.MX6s - building Xorg on Ltib: libX11 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6s - building Xorg on Ltib: libX11 problem

1,337 Views
mirogliopaolo
Contributor II

Dear Sirs,

I'm encountering problem when building libX11 for Xorg on i.mx6s, i'm using the L3.0.35_3.0.0_121207 source on a Centos OS 6.4.

.spec file and all other configurations are kept by standard, on ltib mode i just selected "Build full modular", but also manually selection of this library is going wrong.

PLease check below the building process, it stops on the final part of the build, problem regards following objects:

xlibi18n/libi18n.a

xcms/libxcms.a

xkb/libxkb.a

as i can see from the last part of the build comand:

,--whole-archive xlibi18n/.libs/libi18n.a xcms/.libs/libxcms.a xkb/.libs/libxkb.a -Wl,--no-whole-archive  -L/sw/ltib/rootfs/usr/lib -lxcb-xlib -lxcb -ldl  -Wl,-soname -Wl,libX11.so.6 -o .libs/libX11.so.6.2.0

xlibi18n/.libs/libi18n.a: member xlibi18n/.libs/libi18n.a(lcSjis.o) in archive is not an object

I made already distclean and so on but nothing changes, so i think there is something unhandled in the makefile generation in the ./src or ./src/libi18n folders.

I'm trying to understand what can cause this problem, any help or suggestion could be helpful.

/bin/sh ../libtool --tag=CC   --mode=link gcc -I../include -I../include/X11 -I../include -I../include/X11 -I../src/xcms -I../src/xkb -I../src/xlibi18n -Wall -Wpointer-arith -Wstrict-prototypes     -Wmissing-prototypes -Wmissing-declarations     -Wnested-externs -fno-strict-aliasing -D_BSD_SOURCE -DHAS_FCHOWN -DHAS_STICKY_DIR_BIT -I/sw/ltib/rootfs/usr/include-I/sw/ltib/rootfs/usr/include   -I/sw/ltib/rootfs/usr/include   -I/sw/ltib/rootfs/usr/include-D_BSD_SOURCE -DX11_t -DTRANS_CLIENT -DMALLOC_0_RETURNS_NULL -g -O2 -version-number 6:2:0 -no-undefined  -o libX11.la -rpath /usr/lib AllCells.lo AllowEv.lo AllPlanes.lo AutoRep.lo Backgnd.lo BdrWidth.lo Bell.lo Border.lo ChAccCon.lo ChActPGb.lo ChClMode.lo ChCmap.lo ChGC.lo ChKeyCon.lo ChkIfEv.lo ChkMaskEv.lo ChkTypEv.lo ChkTypWEv.lo ChkWinEv.lo ChPntCon.lo ChProp.lo ChSaveSet.lo ChWAttrs.lo ChWindow.lo CirWin.lo CirWinDn.lo CirWinUp.lo ClDisplay.lo ClearArea.lo Clear.lo ConfWind.lo Context.lo ConvSel.lo CopyArea.lo CopyCmap.lo CopyGC.lo CopyPlane.lo CrBFData.lo CrCmap.lo CrCursor.lo CrGC.lo CrGlCur.lo CrPFBData.lo CrPixmap.lo CrWindow.lo Cursor.lo DefCursor.lo DelProp.lo Depths.lo DestSubs.lo DestWind.lo DisName.lo DrArc.lo DrArcs.lo DrLine.lo DrLines.lo DrPoint.lo DrPoints.lo DrRect.lo DrRects.lo DrSegs.lo ErrDes.lo ErrHndlr.lo evtomask.lo EvToWire.lo FetchName.lo FillArc.lo FillArcs.lo FillPoly.lo FillRct.lo FillRcts.lo FilterEv.lo Flush.lo Font.lo FontInfo.lo FontNames.lo FreeCmap.lo FreeCols.lo FreeCurs.lo FreeEData.lo FreeGC.lo FreePix.lo FSSaver.lo FSWrap.lo GCMisc.lo Geom.lo GetAtomNm.lo GetColor.lo GetDflt.lo GetFPath.lo GetFProp.lo GetGCVals.lo GetGeom.lo GetHColor.lo GetHints.lo GetIFocus.lo GetImage.lo GetKCnt.lo GetMoEv.lo GetNrmHint.lo GetPCnt.lo GetPntMap.lo GetProp.lo GetRGBCMap.lo GetSOwner.lo GetSSaver.lo GetStCmap.lo GetTxtProp.lo GetWAttrs.lo GetWMCMapW.lo GetWMProto.lo globals.lo GrButton.lo GrKeybd.lo GrKey.lo GrPointer.lo GrServer.lo Host.lo Iconify.lo IfEvent.lo imConv.lo ImText16.lo ImText.lo ImUtil.lo InitExt.lo InsCmap.lo IntAtom.lo KeyBind.lo KeysymStr.lo KillCl.lo LiHosts.lo LiICmaps.lo LiProps.lo ListExt.lo LoadFont.lo LockDis.lo locking.lo LookupCol.lo LowerWin.lo Macros.lo MapRaised.lo MapSubs.lo MapWindow.lo MaskEvent.lo Misc.lo ModMap.lo MoveWin.lo NextEvent.lo OCWrap.lo OMWrap.lo OpenDis.lo ParseCmd.lo ParseCol.lo ParseGeom.lo PeekEvent.lo PeekIfEv.lo Pending.lo PixFormats.lo PmapBgnd.lo PmapBord.lo PolyReg.lo PolyTxt16.lo PolyTxt.lo PropAlloc.lo PutBEvent.lo PutImage.lo Quarks.lo QuBest.lo QuColor.lo QuColors.lo QuCurShp.lo QuExt.lo QuKeybd.lo QuPntr.lo QuStipShp.lo QuTextE16.lo QuTextExt.lo QuTileShp.lo QuTree.lo RaiseWin.lo RdBitF.lo RecolorC.lo ReconfWin.lo ReconfWM.lo Region.lo RegstFlt.lo RepWindow.lo RestackWs.lo RotProp.lo ScrResStr.lo SelInput.lo SendEvent.lo SetBack.lo SetClMask.lo SetClOrig.lo SetCRects.lo SetDashes.lo SetFont.lo SetFore.lo SetFPath.lo SetFunc.lo SetHints.lo SetIFocus.lo SetLocale.lo SetLStyle.lo SetNrmHint.lo SetPMask.lo SetPntMap.lo SetRGBCMap.lo SetSOwner.lo SetSSaver.lo SetState.lo SetStCmap.lo SetStip.lo SetTile.lo SetTSOrig.lo SetTxtProp.lo SetWMCMapW.lo SetWMProto.lo StBytes.lo StColor.lo StColors.lo StName.lo StNColor.lo StrKeysym.lo StrToText.lo Sync.lo Synchro.lo Text16.lo Text.lo TextExt16.lo TextExt.lo TextToStr.lo TrCoords.lo UndefCurs.lo UngrabBut.lo UngrabKbd.lo UngrabKey.lo UngrabPtr.lo UngrabSvr.lo UninsCmap.lo UnldFont.lo UnmapSubs.lo UnmapWin.lo VisUtil.lo WarpPtr.lo Window.lo WinEvent.lo Withdraw.lo WMGeom.lo WMProps.lo WrBitF.lo XlibAsync.lo XlibInt.lo Xrm.loxcb_lock.lo xcb_disp.lo xcb_io.lo  xlibi18n/libi18n.la xcms/libxcms.la xkb/libxkb.la -L/sw/ltib/rootfs/usr/lib -lxcb-xlib -lxcb  -ldl

gcc -shared  .libs/AllCells.o .libs/AllowEv.o .libs/AllPlanes.o .libs/AutoRep.o .libs/Backgnd.o .libs/BdrWidth.o .libs/Bell.o .libs/Border.o .libs/ChAccCon.o .libs/ChActPGb.o .libs/ChClMode.o .libs/ChCmap.o .libs/ChGC.o .libs/ChKeyCon.o .libs/ChkIfEv.o .libs/ChkMaskEv.o .libs/ChkTypEv.o .libs/ChkTypWEv.o .libs/ChkWinEv.o .libs/ChPntCon.o .libs/ChProp.o .libs/ChSaveSet.o .libs/ChWAttrs.o .libs/ChWindow.o .libs/CirWin.o .libs/CirWinDn.o .libs/CirWinUp.o .libs/ClDisplay.o .libs/ClearArea.o .libs/Clear.o .libs/ConfWind.o .libs/Context.o .libs/ConvSel.o .libs/CopyArea.o .libs/CopyCmap.o .libs/CopyGC.o .libs/CopyPlane.o .libs/CrBFData.o .libs/CrCmap.o .libs/CrCursor.o .libs/CrGC.o .libs/CrGlCur.o .libs/CrPFBData.o .libs/CrPixmap.o .libs/CrWindow.o .libs/Cursor.o .libs/DefCursor.o .libs/DelProp.o .libs/Depths.o .libs/DestSubs.o .libs/DestWind.o .libs/DisName.o .libs/DrArc.o .libs/DrArcs.o .libs/DrLine.o .libs/DrLines.o .libs/DrPoint.o .libs/DrPoints.o .libs/DrRect.o .libs/DrRects.o .libs/DrSegs.o .libs/ErrDes.o .libs/ErrHndlr.o .libs/evtomask.o .libs/EvToWire.o .libs/FetchName.o .libs/FillArc.o .libs/FillArcs.o .libs/FillPoly.o .libs/FillRct.o .libs/FillRcts.o .libs/FilterEv.o .libs/Flush.o .libs/Font.o .libs/FontInfo.o .libs/FontNames.o .libs/FreeCmap.o .libs/FreeCols.o .libs/FreeCurs.o .libs/FreeEData.o .libs/FreeGC.o .libs/FreePix.o .libs/FSSaver.o .libs/FSWrap.o .libs/GCMisc.o .libs/Geom.o .libs/GetAtomNm.o .libs/GetColor.o .libs/GetDflt.o .libs/GetFPath.o .libs/GetFProp.o .libs/GetGCVals.o .libs/GetGeom.o .libs/GetHColor.o .libs/GetHints.o .libs/GetIFocus.o .libs/GetImage.o .libs/GetKCnt.o .libs/GetMoEv.o .libs/GetNrmHint.o .libs/GetPCnt.o .libs/GetPntMap.o .libs/GetProp.o .libs/GetRGBCMap.o .libs/GetSOwner.o .libs/GetSSaver.o .libs/GetStCmap.o .libs/GetTxtProp.o .libs/GetWAttrs.o .libs/GetWMCMapW.o .libs/GetWMProto.o .libs/globals.o .libs/GrButton.o .libs/GrKeybd.o .libs/GrKey.o .libs/GrPointer.o .libs/GrServer.o .libs/Host.o .libs/Iconify.o .libs/IfEvent.o .libs/imConv.o .libs/ImText16.o .libs/ImText.o .libs/ImUtil.o .libs/InitExt.o .libs/InsCmap.o .libs/IntAtom.o .libs/KeyBind.o .libs/KeysymStr.o .libs/KillCl.o .libs/LiHosts.o .libs/LiICmaps.o .libs/LiProps.o .libs/ListExt.o .libs/LoadFont.o .libs/LockDis.o .libs/locking.o .libs/LookupCol.o .libs/LowerWin.o .libs/Macros.o .libs/MapRaised.o .libs/MapSubs.o .libs/MapWindow.o .libs/MaskEvent.o .libs/Misc.o .libs/ModMap.o .libs/MoveWin.o .libs/NextEvent.o .libs/OCWrap.o .libs/OMWrap.o .libs/OpenDis.o .libs/ParseCmd.o .libs/ParseCol.o .libs/ParseGeom.o .libs/PeekEvent.o .libs/PeekIfEv.o .libs/Pending.o .libs/PixFormats.o .libs/PmapBgnd.o .libs/PmapBord.o .libs/PolyReg.o .libs/PolyTxt16.o .libs/PolyTxt.o .libs/PropAlloc.o .libs/PutBEvent.o .libs/PutImage.o .libs/Quarks.o .libs/QuBest.o .libs/QuColor.o .libs/QuColors.o .libs/QuCurShp.o .libs/QuExt.o .libs/QuKeybd.o .libs/QuPntr.o .libs/QuStipShp.o .libs/QuTextE16.o .libs/QuTextExt.o .libs/QuTileShp.o .libs/QuTree.o .libs/RaiseWin.o .libs/RdBitF.o .libs/RecolorC.o .libs/ReconfWin.o .libs/ReconfWM.o .libs/Region.o .libs/RegstFlt.o .libs/RepWindow.o .libs/RestackWs.o .libs/RotProp.o .libs/ScrResStr.o .libs/SelInput.o .libs/SendEvent.o .libs/SetBack.o .libs/SetClMask.o .libs/SetClOrig.o .libs/SetCRects.o .libs/SetDashes.o .libs/SetFont.o .libs/SetFore.o .libs/SetFPath.o .libs/SetFunc.o .libs/SetHints.o .libs/SetIFocus.o .libs/SetLocale.o .libs/SetLStyle.o .libs/SetNrmHint.o .libs/SetPMask.o .libs/SetPntMap.o .libs/SetRGBCMap.o .libs/SetSOwner.o .libs/SetSSaver.o .libs/SetState.o .libs/SetStCmap.o .libs/SetStip.o .libs/SetTile.o .libs/SetTSOrig.o .libs/SetTxtProp.o .libs/SetWMCMapW.o .libs/SetWMProto.o .libs/StBytes.o .libs/StColor.o .libs/StColors.o .libs/StName.o .libs/StNColor.o .libs/StrKeysym.o .libs/StrToText.o .libs/Sync.o .libs/Synchro.o .libs/Text16.o .libs/Text.o .libs/TextExt16.o .libs/TextExt.o .libs/TextToStr.o .libs/TrCoords.o .libs/UndefCurs.o .libs/UngrabBut.o .libs/UngrabKbd.o .libs/UngrabKey.o .libs/UngrabPtr.o .libs/UngrabSvr.o .libs/UninsCmap.o .libs/UnldFont.o .libs/UnmapSubs.o .libs/UnmapWin.o .libs/VisUtil.o .libs/WarpPtr.o .libs/Window.o .libs/WinEvent.o .libs/Withdraw.o .libs/WMGeom.o .libs/WMProps.o .libs/WrBitF.o .libs/XlibAsync.o .libs/XlibInt.o .libs/Xrm.o .libs/xcb_lock.o .libs/xcb_disp.o .libs/xcb_io.o -Wl,--whole-archive xlibi18n/.libs/libi18n.a xcms/.libs/libxcms.a xkb/.libs/libxkb.a -Wl,--no-whole-archive  -L/sw/ltib/rootfs/usr/lib -lxcb-xlib -lxcb -ldl  -Wl,-soname -Wl,libX11.so.6 -o .libs/libX11.so.6.2.0

xlibi18n/.libs/libi18n.a: member xlibi18n/.libs/libi18n.a(lcSjis.o) in archive is not an object

collect2: ld returned 1 exit status

make[3]: *** [libX11.la] Error 1

make[3]: Leaving directory `/sw/ltib/rpm/BUILD/libX11-1.1.5/src'

make[2]: *** [all-recursive] Error 1

make[2]: Leaving directory `/sw/ltib/rpm/BUILD/libX11-1.1.5/src'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/sw/ltib/rpm/BUILD/libX11-1.1.5/src'

make: *** [all-recursive] Error 1

error: Bad exit status from /sw/ltib/tmp/rpm-tmp.98598 (%build)


5 Replies

805 Views
mirogliopaolo
Contributor II

Compilation run succesfully by just changing Makefile.in inside every dir with that error:

am_ximcp_la_OBJECTS = ...list of .lo files...

i renamed all listed files from .lo extension to .o and libtool correctly build the objects and generates the shared library.

Paolo

805 Views
LeonardoSandova
Specialist I

Paolo,

would you mind comparing this particular spec with the one coming with the latest BSP for iMX6Q? We may find the reason of this compilation issue.

Leo

0 Kudos

805 Views
mirogliopaolo
Contributor II

Dear Leonardo,

thanks for your answer.

Do you mean the ltib libX11 .spec file? I'm using the original from freescale (121207) source.

Using --disable-shared at configure time build ends well but obviously does not generate the shared library libX11 that is needed, so i take back the original .spec file.

I also discovered that the error "archive is not an object" regarding some .o files is because those object files are of ZERO length in bytes, while the .lo files seems to be generated correctly.

Problem of 0bytes length on some .o files is happening on following subdirs:

/sw/ltib/rpm/BUILD/libX11-1.1.5/src/xlibi18n

/sw/ltib/rpm/BUILD/libX11-1.1.5/src/xcms

Maybe some configure,Makefile,libtool script problem?

I'll continue investigation, if any idea it would be kind a suggestion...


Miroglio Paolo





0 Kudos

805 Views
LeonardoSandova
Specialist I

Yes. that is what I meant. Compare libX11 .spec file between your BSP and the latest BSP from the iMX6Q board (version 1.1.0). Also, next time you do a build, please remove the rpm/BUILD/libX-... so you start with a fresh build.

Leo

0 Kudos

805 Views
mirogliopaolo
Contributor II

Dear Leo,

.spec files after diff are the same (checked on dual/quad L3.0.35_1.1.0_121218_source.tar.gz), also source is the same: libX11-1.1.5

I always delete the folder in /BUILD, tried also with ./ltib -m distclean.

I'll continue to investigate but i still haven't found a solution...thank you again.


Paolo

0 Kudos