Return mode on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Return mode on iMX6

Jump to solution
5,391 Views
AlbertT
Contributor V

Hello !

I was wondering what exactly is the return mode which is present on the iMX6 ? I think it's also called FSL mode, the reference manual mention it but doesn't really describe what it is and what we can do with it. It seems to be something between open and closed mode.

Regards,

Jocelyn Kevorkian

Labels (2)
0 Kudos
Reply
1 Solution
4,834 Views
Yuri
NXP Employee
NXP Employee

The FIELD RETURN mode is described in the i.MX6 Security Reference Manual.

View solution in original post

8 Replies
4,835 Views
Yuri
NXP Employee
NXP Employee

The FIELD RETURN mode is described in the i.MX6 Security Reference Manual.

4,834 Views
AlbertT
Contributor V

Yep I found it after !

0 Kudos
Reply
4,834 Views
AlbertT
Contributor V

Well, ok then.

Thanks.

0 Kudos
Reply
4,834 Views
Yuri
NXP Employee
NXP Employee

In the field return mode Security configuration - is as Open, also FSL Test modes are re-enabled
to allow device testing.

4,834 Views
AlbertT
Contributor V

Hello Yuri,

Ok thanks ! Is there a document where I can find more details about FSL tests modes ?

0 Kudos
Reply
4,834 Views
Yuri
NXP Employee
NXP Employee

Alas, I never seen FSL tests description.  

0 Kudos
Reply
4,834 Views
AlbertT
Contributor V

Hello Fabio,

On page 454 of the RM, we have the description of boot security settings, there are open/closed/field return which is described by "This level is intended for parts returned from shipped products".

On page 456, an eFuse is called FIELD_RETURN and its definition is "Enables FSL reserved modes".

So I would like to know what is field return, and how we can use it ?
Thanks !

Jocelyn Kevorkian

0 Kudos
Reply
4,834 Views
fabio_estevam
NXP Employee
NXP Employee

Can you provide more context to your question? I am not able to understand what you are asking with your current description.

0 Kudos
Reply