Response to unsigned binary in secure boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Response to unsigned binary in secure boot

ソリューションへジャンプ
2,044件の閲覧回数
eren_yilmaz
Contributor III

Hi,

Does a SecureBoot-enabled device get bricked if one flashes a regular image (not signed) onto it? What is the response of the processor to a .bin that is not signed or signed with incorrect keys? Does it simply raise HAB events at boot level and wait for a signed image to be flashed?

Thanks

ラベル(3)
0 件の賞賛
返信
1 解決策
1,964件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  All along the boot  procedure and until the boot image is executed, the HAB logs the

encountered errors and warnings. If the boot fails - secure serial bootloader (SDP) 

starts.

Have a great day,

Yuri

 

 -------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

1 返信
1,965件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  All along the boot  procedure and until the boot image is executed, the HAB logs the

encountered errors and warnings. If the boot fails - secure serial bootloader (SDP) 

starts.

Have a great day,

Yuri

 

 -------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.