Resetvector catch in iMX8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Resetvector catch in iMX8QM

3,055 次查看
ranjith_tc
Contributor I

Hi,

In the iMX8QM, I am trying to do a reset catch.

For this I am setting the EDECR.RCE to 1 and necessary steps to do the warm reset from software( RMR_ELn.RR=1).

The target is gettting reset, but it is not stopping at reset vector.

Do i  need to do anything else to make this happen?

Regards,

ranjith

@‌igorpadykov

0 项奖励
回复
5 回复数

2,994 次查看
ranjith_tc
Contributor I

Hi Igor,

I would like to reset the first A53 core and halt it at the reset vector.

For this I am using the RMR_EL2.RR bit.and for catching at the reset, I am setting EDECR.RCE bit.

The core is getting reset and it starts running. So when i check thestatus of EDECR, it has been cleared.

What kind of reset it do when RR is set? A warm reset or cold reset? If it is a warm reset the register should not clear isnt it?

Is ARMv8-A DoPD is implemented in iMX8QM? If it is not, EDECR comes in Debug power domain as per ARM v8-A specification.

So it should not clear even if a cold reset is done. What could be the reason for the register is getting reset?

Regards,

Ranjith

0 项奖励
回复

2,994 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

in i.MX8 series it is not possible to manipulate A53 core directly, it is done through SCU

System Controller Unit (SCU) Introduction for i.MX 8QXP MEK - i.MXDev Blog 

Best regards
igor

0 项奖励
回复

2,992 次查看
ranjith_tc
Contributor I

HI,

Thanks Igor for the support.

So, is ther any way to halt the the A53 cores at reset vector in iMX8QM?

regards.

Ranjith

0 项奖励
回复

2,992 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

one can look at documentation included in SCFW Porting Kit

for available reset options.

Best regards
igor

0 项奖励
回复

2,992 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

for reset examples one can look at:

imx8.c\platform\user - m4ctrl - M4 Control Tool for i.MX platforms 

Please be aware of partition reset. This will reset only a part of the SoC. It does not rerun the ROM
so code will not be reloaded. By default ATF does a partition reset, not a board reset.

https://community.nxp.com/docs/DOC-341481 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复