MX8QXP输出1路RGB,2路LVDS,能不能驱动双屏,分辨率都是1920*720,每个屏需要2路LVDS,共需要4路LVDS
i.mx8x can support dual display:
The Display controller subsystem supports two Display Controllers (DC0 and DC1).
The DC can generate the output video timing for one display with image content read from the display buffers in the memory and/or directly captured input video timing.
The Display Controller 0 (DC0) interfaces the following blocks:
- Two LVDS interfaces supporting
- 1080p@60 on a single interface
- 4k@30 when aggregating the two interfaces
The Display Controller 1 (DC1) interfaces the following blocks:
- Two LVDS interfaces supporting
- 1080p@60 on a single interface
- 4k@30 when aggregating the two interfaces