Reset virtio_rpmsg_bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reset virtio_rpmsg_bus

跳至解决方案
6,382 次查看
dogisfat
Contributor IV

I am trying to figure out how to reinitialize/reset the virtio_rpmsg_bus. I have an application where the m4 is loaded from linux which communicates with rpmsg. The issues I have is the virtqueues hold all of the old messages causing the m4 to read all of the old message erroneously. How can I reset the virtio bus to a fresh state?

标记 (1)
0 项奖励
回复
1 解答
5,768 次查看
dogisfat
Contributor IV

I was able to get the virtio bus to reset by making it a loadable module. When the module is removed and probed all of the memory gets cleaned up/reallocated. I had to change the Kconfig and Makefile that reside adjacent to virtio_rpmsg_bus to be as follows.

Kconfig:

menu "Rpmsg drivers"

# RPMSG always gets selected by whoever wants it
config RPMSG
     tristate
     select VIRTIO
     select VIRTUALIZATION

config IMX_VIRTIO_RPMSG_BUS
     tristate "IMX RPMSG virtio rpmsg bus -- lodable modules only"
     default m
     depends on RPMSG && m

config IMX_RPMSG_PINGPONG
     tristate "IMX RPMSG pingpong driver -- loadable modules only"
     default m
     depends on RPMSG && m && IMX_VIRTIO_RPMSG_BUS

config IMX_RPMSG_TTY
     tristate "IMX RPMSG tty driver -- loadable modules only"
     default m
     depends on RPMSG && m && IMX_VIRTIO_RPMSG_BUS

endmenu
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Makefile:

obj-$(CONFIG_IMX_VIRTIO_RPMSG_BUS)     += virtio_rpmsg_bus.o
obj-$(CONFIG_IMX_RPMSG_PINGPONG)     += imx_rpmsg_pingpong.o
obj-$(CONFIG_IMX_RPMSG_TTY)     += imx_rpmsg_tty.o
‍‍‍

在原帖中查看解决方案

3 回复数
5,769 次查看
dogisfat
Contributor IV

I was able to get the virtio bus to reset by making it a loadable module. When the module is removed and probed all of the memory gets cleaned up/reallocated. I had to change the Kconfig and Makefile that reside adjacent to virtio_rpmsg_bus to be as follows.

Kconfig:

menu "Rpmsg drivers"

# RPMSG always gets selected by whoever wants it
config RPMSG
     tristate
     select VIRTIO
     select VIRTUALIZATION

config IMX_VIRTIO_RPMSG_BUS
     tristate "IMX RPMSG virtio rpmsg bus -- lodable modules only"
     default m
     depends on RPMSG && m

config IMX_RPMSG_PINGPONG
     tristate "IMX RPMSG pingpong driver -- loadable modules only"
     default m
     depends on RPMSG && m && IMX_VIRTIO_RPMSG_BUS

config IMX_RPMSG_TTY
     tristate "IMX RPMSG tty driver -- loadable modules only"
     default m
     depends on RPMSG && m && IMX_VIRTIO_RPMSG_BUS

endmenu
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Makefile:

obj-$(CONFIG_IMX_VIRTIO_RPMSG_BUS)     += virtio_rpmsg_bus.o
obj-$(CONFIG_IMX_RPMSG_PINGPONG)     += imx_rpmsg_pingpong.o
obj-$(CONFIG_IMX_RPMSG_TTY)     += imx_rpmsg_tty.o
‍‍‍
5,768 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Allen,

virtio_rpmsg_bus is not NXP exclusive. You can look at generic virtio infromation such as this: https://www.kernel.org/doc/Documentation/rpmsg.txt 

For running RPmsg demo in NXP i.MX devices you can have a look here: Running RPMsg Demo Applications for Multicore Communication with IMX6SX and IMX7D 


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,768 次查看
dogisfat
Contributor IV

Carlos,

I am able to run the demo without issue. I also have read the rpmsg documentation provided at kernel.org. There is also the imx_rpmsg.c implementation backing virtio_rpmsg_bus which *is* NXP exclusive. One of the calls exposed in imx_rpmsg.c is imx_rpmsg_reset which is just stubbed out to print "reset !" instead of performing a bus reset. I don't want to seem attacking or mean but neither of your comments seem like they help the community at large as both are easily googleable. The question at hand however could prove useful to others and doesn't have an easily searchable solution.

Thanks,

Allen

0 项奖励
回复