Request for support on achieving two simultaneus display using embedded linux for NXP i.MX processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for support on achieving two simultaneus display using embedded linux for NXP i.MX processor

1,112件の閲覧回数
Rama1
Contributor I

Dear NXP Semiconductors,

I am writing to request support on how to achieve two simultaneous display using embedded linux for NXP i.MX processors. I am interested in using embedded linux to run two separate displays (XGA + VGA) simultaneously for either i.MX6Q/i.MX8MQ.

From the i.MX processor datasheet, it shows that up to 4 simultaneous displays are supported, and I assume, corresponding display driver and framework (weston / X11) are enabled in NXP i.MX linux to achieve simultaneous displays.

I would be great if I could get the steps to achieve two simultaneous display using i.MX linux. 

Thank you

0 件の賞賛
返信
1 返信

1,090件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for imx8mq, current bsp support dual display(HDMI+mipi dsi) already, customer doesn't need to change anything, for more detailed information, you can refer to the dts file

"https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mq-evk-dual-dis..."

0 件の賞賛
返信