Dear Forum members,
i am trying to bring up display on iMx8mm processor board using raydium-rm68200 driver (drivers/gpu/drm/panel/panel-raydium-rm68200.c) in 5.10 kernel.
Earlier discussed one of the issue specific to rm68200 panel driver in below link. one of the comment mentioned dts file is attached for rm68200 panel but it's not attached in the zip file mentioned in one of the comments.
Re: MIPI DSI LCD display in i.MX8M - NXP Community
Request to share rm68200 panel dts file for reference?
Regards
Nela
解決済! 解決策の投稿を見る。
done with it. closing.
Done with it. closing.
Hi @koteswararao18!
Thank you for contacting NXP Support!
You can check the next device tree for reference:
Is compatible with the next display:
Best Regards!
Chavira
Dear chavira
Thank you so much for your input.
>>https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8ulp-evk-rk055...
Referred above dts file and prepare/built successfully rm68200 panel dts file.
Now, For the customized LCD Panel (GH8555BLV) at my desk, it uses rm68200 panel driver along with initialization of below registers 0x11 and 0x29.
{{
DSI_CMD(0x11,0,0x00); //Sleep Out
DelayX1ms(150);
DSI_CMD(0x29,0,0x00); //Display On
DelayX1ms(50);
}}
How to add above piece of registers initialization code during initialization phase in rm68200 display panel code.
(drivers/gpu/drm/panel/panel-raydium-rm68200.c)(kernel version-5.10)
Referred below link
https://forums.raspberrypi.com/viewtopic.php?t=332609 for register initialization but not didn't help much.
please do let me know if you have inputs about it.
Regards
Nela