Request for i.MX535 Performance Benchmark Document

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for i.MX535 Performance Benchmark Document

1,179 Views
SrideviK
Contributor III

Hi,

Pls share the i.MX535 Performance Document or Report (either Sabre / EVK) for our benchmarking.

Need to understand the peripheral access speed achieved for Micro-SD/eMMC/USB, etc.

Regards,

Sridevi

0 Kudos
Reply
2 Replies

1,074 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Sridevi,

You can go to http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&... to download the IMX53RM. The details of performance and peripheral speed access you can see in it. Hope this can help you ~~

Best Regards

Dan


0 Kudos
Reply

1,074 Views
SrideviK
Contributor III

Thanks Dan for the reply.

My device is based on i.MX535 (Android2.3.7 platform). The design is done almost similar to the i.MX535 based Sabre / QSB.

I need to evaluate the performance of all the interfaces in my device.

For this I would need the practical performance report for the processor interfaces - so i.MX535 based Sabre / QSB performance report would be suitable for the same.

Hope the interface performances would have been evaluated using some tools.

Pls share the relevant document for benchmarking.

Regards,

Sridevi

0 Kudos
Reply