Request for Support on i.MX6SX Board Bring-Up and Device Tree Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Request for Support on i.MX6SX Board Bring-Up and Device Tree Configuration

451 次查看
Ajay333
Contributor I

Hello,

I am currently involved in the board bring-up process for our NXP i.MX6SX EVB 3 board.

Since I plan to run Linux on this board for our custom application, I attempted to boot it using the latest U-Boot version for the i.MX6 SoloX processor. However, when using the new U-Boot binary, there was no output on the UART console, suggesting that the boot process was failing very early—possibly during DDR initialization.

To debug this, I compared the working GAPI firmware (provided by NXP) with the new U-Boot image and found differences in the IVT (Image Vector Table) header, particularly in the DCD (Device Configuration Data) section, which is responsible for DDR memory initialization.

As an experiment, I kept the DCD section from the GAPI firmware and replaced only the U-Boot portion with the latest version. With this configuration, the board was able to boot, and I received the following output:

U-Boot 2024.04-lf_v2024.04+ge3219a5a734+p0 (Feb 18 2025 - 04:03:02 +0000)
CPU: i.MX6SX rev1.3 at 792MHz
Model: i.MX6 SoloX Sabre Auto Board
DRAM: 128 MiB
pca953x gpio@30: Error reading output register
pca953x gpio@32: Error reading output register
initcall failed at call 86eb8ff9 (err=-22)
### ERROR ### Please RESET the board ###

In addition, I also tried booting the board using Yocto-generated images, but encountered the same issue—no UART output and no successful boot. So far, the board only boots reliably when using the full GAPI image from NXP, which includes the correct DCD configuration.

We now have access to the board schematics, Could you assist us in identifying or generating the correct DCD settings for this board? Any guidance on customizing the U-Boot DCD table or using NXP tools for DDR configuration based on the schematics would be greatly appreciated.



标签 (1)
0 项奖励
回复
1 回复

423 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Ajay333 

I hope you are doing very well.

 

It appears this topic is duplicated, the original post is:

 

https://community.nxp.com/t5/i-MX-Processors/Request-for-Guidance-on-i-MX6SX-Board-Bring-Up-and-Devi...

 

Please contact to your DFAE or Sales person if you have more questions.

 

Best regards,

Salas.

0 项奖励
回复