Request for Linux Kernel Driver Support for TEF3200HN/V205Y Tuner

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Linux Kernel Driver Support for TEF3200HN/V205Y Tuner

831 Views
Joseph_Chiristopher_N
Contributor II

Hello NXP Team,

I'm currently working on a custom Linux BSP for the i.MX6SX-sdb processor and would like to interface the TEF3200HN/V205Y DAB tuner chip via I2C.

Could you please provide:

  1. A Linux kernel driver (or reference driver) for the TEF3200HN?
  2. The appropriate compatible string and any required device tree bindings.
  3. Any documentation regarding register map, initialization sequences, or I2C protocol for the TEF3200HN.

For example, in my device tree, I'm planning something along the lines of:

&i2c1 {
clock-frequency = <100000>;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c1>;

tef3200: tef3200@60 {
compatible = "nxp,tef3200hn";
reg = <0x60>;
status = "okay";
/* Add GPIOs, supplies, clocks here if required */
};
};

I'm currently using Linux kernel 6.12.3-lts-next
 and Yocto-based build system.

Looking forward to your support.

Thank You,

0 Kudos
Reply
1 Reply

816 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @Joseph_Chiristopher_N 

you need to contact the  TEF3200HN/V205Y vendor provide the related driver code file. 

B.R

0 Kudos
Reply