Request for Documentation on Interfaces Supported in OpenWRT for i.MX93 Platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for Documentation on Interfaces Supported in OpenWRT for i.MX93 Platform

999件の閲覧回数
Dheeraj_8
Contributor I

Hello,

I am working with the i.MX93 platform using OpenWRT and need detailed documentation or a user manual listing all the interfaces supported (e.g., USB, Ethernet, LCDIF, MIPI, etc.) in this platform's OpenWRT environment.

Specifically, I am looking for information on how these interfaces are configured and integrated, along with any related device tree configurations or examples. Any guidance or pointers to relevant documents, user manuals, or reference materials would be greatly appreciated.

0 件の賞賛
返信
4 返答(返信)

966件の閲覧回数
Dheeraj_8
Contributor I
Hello,

Thank you for sharing the links. I am interested in understanding the specific features and interfaces supported by OpenWRT on the NXP  platform. Could you please provide more details about the supported hardware interfaces (such as Ethernet, USB, I2C, SPI, etc.) and any other features that are implemented or available for customization in the OpenWRT environment 

Looking forward to your response.

Best regards,

 

0 件の賞賛
返信

962件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can view the features and installation here:. Some one update the User guide for OpenWrt support on i.MX6 platform. still now i use 

1.https://oldwiki.archive.openwrt.org/doc/devel/add.new.platform 

2.https://wiki.dd-wrt.com/wiki/index.php?title=Special:PdfPrint&page=Optware_on_K3-AC-ARM/Repositories 

don't have official user guide for this, but maybe you can refer to the porting document which is posted by the other customer:

https://blog.csdn.net/wind0419/article/details/78036522

Regards

 

0 件の賞賛
返信

938件の閲覧回数
Dheeraj_8
Contributor I

Hello,

Thank you for the resources shared. I hope you might have already tested OpenWRT on the i.MX93 platform. Could you please share the supported features and interfaces for OpenWRT on i.MX93? How do they compare to the standard Linux setup on the i.MX93? Is it the same, or are there any differences in terms of hardware support or drivers?

Additionally, I noticed that in the hardware table model list which is attched below, I couldn't find a model related to i.MX. Could you kindly help clarify if there is any entry for i.MX93 or similar in the list?

Dheeraj_8_0-1736143536865.png
Regards

 

0 件の賞賛
返信

981件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no document about OpenWRT and MX93, however it is supported you migth check:

https://community.nxp.com/t5/i-MX-Processors/OpenWRT-i-MX8-Customize/m-p/1758230

https://git.openwrt.org/?a=project_list;pf=openwrt

mx openwrt source code:

https://github.com/nxp-imx/imx_openwrt/

Regards

0 件の賞賛
返信