Removing Psplash from image(IMX6Q)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Removing Psplash from image(IMX6Q)

6,131件の閲覧回数
mustafabakircio
Contributor IV

Hello Guys;

I want to remove the yocto project loading screen from the image . I couldnt find any way to this . Would it be possible to remove from perminently from the  U-boot console or directly from the image ?

Screenshot from 2017-06-19 10-55-02.png

4 返答(返信)

5,147件の閲覧回数
nandishguruling
Contributor III

Hi Mustafa,

Thanks for your reply, we no need to delete any file, we need to do just change file i.e *-img.h , with conversion thats it,

Thanks & Best Regards,

nandish sg

0 件の賞賛
返信

5,147件の閲覧回数
nandishguruling
Contributor III

Hi Mustafa,

Have you done this task, if not please let me know,

Best Regards

Nandish SG

0 件の賞賛
返信

5,147件の閲覧回数
mustafabakircio
Contributor IV

Hi @nandish gurulingappa

At this directory  source/poky/meta-yocto/recipes-core/psplash you can change the plasplash_git.bbappend file or you can delete it . But when I do that I faced with this image , it so funny :smileygrin:

20171012_173425.jpg

I thing there are more about psplash image in /source directory. You need to check them and delete after that it could be done I guess.

5,147件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信