Remove Cursor pointer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Remove Cursor pointer

14,441件の閲覧回数
enaud
Contributor III

Hi,

How remove mouse cursor from my application?

ラベル(1)
11 返答(返信)

9,957件の閲覧回数
erickang
Contributor II

Hi Giuseppe Ventura,

echo 0 > /sys/class/graphics/fbcon/cursor_blink

- cursor hide

   ~ $ echo -e '\033[?17;0;0c' > /dev/tty1

But I couldn't remove the cursor.

I could see the black cursor position not to be removed.

In other words, I could see the black cursor (not blinking) when I performed the upper command on the white displayed image of LCD.

Could you tell me how to remove the cursor?

And Yuri Muhin,

I could not find the reference site, "Removing the Cursor of LCD framebuffer".

http://www.imxdev.org/wiki/index.php?title=All

Could you give me the correct address for that?

9,957件の閲覧回数
Yuri
NXP Employee
NXP Employee

Removing the Cursor of LCD framebuffer

The Linux framebuffer starts with a cursor on screen, to hides this cursor you can use this command:

echo -e -n '\033[?25l' > /dev/tty0 

9,957件の閲覧回数
erickang
Contributor II

Dear Yuri Muhin,

Thanks for your response.

This command hides the cursor,

but the previous cursor leave a trace with black mark.

I want to remove the black cursor mark.

Could you tell me the method?

Best Regards,

Eric.

0 件の賞賛
返信

9,955件の閲覧回数
erickang
Contributor II

I solved the problem.

For this, I modified the followed files in i.MX25.

(refer to "// Eric" comments in the files)

- No use Cursor Blink

   . drivers/video/console/fbcon.c .

- No display 1st Cursor

    . drivers/video/console/bitblit.c

Best Regards,

Eric.

0 件の賞賛
返信

9,955件の閲覧回数
Vijayaragavan
Contributor I

Hi Eric,

How are you? Nice to see you in the forum.

would like to know how to interface 8bit Dot matric Monochrome LCD with i.mx25 PDK board. Could you please throw some light on this? Lines that we are looking out for interfacing are(LCDC_LD0 to LCDC_LD7) from UF/IF connector(from NVCC_LCDC moudule of i.mx25) and also have no idea how enable them from software.In the existing kernel image we too have fb0 and fb1 devices under /dev diretory. if any sample code is aviable please share some link or please direct me to correct way.

Thanks

0 件の賞賛
返信

9,955件の閲覧回数
enaud
Contributor III

i'veresolved

0 件の賞賛
返信

9,955件の閲覧回数
enaud
Contributor III

up

0 件の賞賛
返信

9,955件の閲覧回数
enaud
Contributor III

up

0 件の賞賛
返信

9,955件の閲覧回数
enaud
Contributor III

thanks but i'm on LVDS display... 

Infact it not work!

0 件の賞賛
返信

9,955件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try the following :

"Removing the Cursor of LCD framebuffer"


http://www.imxdev.org/wiki/index.php?title=All

0 件の賞賛
返信

9,955件の閲覧回数
enaud
Contributor III

nothing?

0 件の賞賛
返信