Removal of PKCS#11 functionality in CST tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Removal of PKCS#11 functionality in CST tool

1,834 Views
pfaust60
Contributor I

I just downloaded the latest CST tool 3.3.1 and found this in the documentation.

The /back_end-hsm directory contains the sources and headers necessary for replacing the open source cryptographic libraries with an implementation that can interact directly with a Hardware Security Module (HSM) by using the PKCS#11 interface definition. More detailed information can be found in the README file located in the directory.
Note: This add-on is deprecated and will be removed in the next CST release.

What will this be replaced with?  Having private keys on the build machine is not a very safe practice.

0 Kudos
Reply
3 Replies

1,821 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @pfaust60 

We will release a safer way to enable HSM in next version.

Regards

Zhiming

0 Kudos
Reply

1,652 Views
Hendrik_M
Contributor I

Is there an update on the status of the new HSM implementation? This is also a pressing matter on my team.

0 Kudos
Reply

1,811 Views
pfaust60
Contributor I

Thanks for the update.  When should we expect a new release and be able to evaluate the new mechanism for integrating with an HSM.

I assume the new solution will still use the industry standard pkcs#11 interface?

Paul Faust

0 Kudos
Reply