Regarding the "Can MFGTOOL program more than one device at once?"  question.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding the "Can MFGTOOL program more than one device at once?"  question.

1,227 Views
peteramond
Contributor V

Hi,

I'm working on a project using imx6 Sabre Lite board. I want know how do I u-boot multiple imx6 Sabre Lite boards at the same time using one single Sd card and how to modify the MFG Tool code.

Regards

Labels (3)
3 Replies

1,087 Views
art
NXP Employee
NXP Employee

The current v.2.xx MFGtool software can service up to 4 devices at a time. You have to specify the number of simultaneously served devices as the PortMgrDlg parameter in the UICfg.ini file (located in the same directory as the executable file).


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,087 Views
peteramond
Contributor V

Does it service 7-8 boards simultaneously? 

0 Kudos
Reply

1,087 Views
art
NXP Employee
NXP Employee

No, no more than 4 boards.

0 Kudos
Reply