Regarding i.MX6SDL IOMUX SPEED field setting.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding i.MX6SDL IOMUX SPEED field setting.

ソリューションへジャンプ
1,552件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL IOMUX pad control.

Please see "SPEED" field in chapter 37.4.212 in IMX6SDLRM Rev.2.

Would you let me know whether there is a difference between the following settings.

01 MEDIUM — 100 MHz, if SRE=1: 100MHz @ 1.8V, 150MHz @ 3.3V

10 MEDIUM — 100 MHz, if SRE=1: 100MHz @ 1.8V, 150MHz @ 3.3V

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 解決策
1,434件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right : settings are the same.

You can ignore my previous remark about exceptions.

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,434件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

there is no difference except few exceptions given in

IMX6SDLRM Table 29-9. IO Operating Frequency

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,434件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Igor,

I checked Table 29-9, but I did not find the difference between SPEED=01b and SPEE=10b.

"Operating Frequency (MHz)" values when SPEED=01b and when SPEED=10b seem to same value regardless of the settings of DSE, SRE, and OVDD.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,435件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right : settings are the same.

You can ignore my previous remark about exceptions.

Best regards

igor

0 件の賞賛
返信