Regarding i.MX6 Linux BSP for year 2038 problem.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Regarding i.MX6 Linux BSP for year 2038 problem.

跳至解决方案
3,777 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ Linux BSP.

You know Linux kernel 3.14 has year 2038 problem.

Would you let me know whether has NXP release a patch for BSP or not?

If not, would you let me know how fix year 2038 problem?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1 解答
3,395 次查看
b36401
NXP Employee
NXP Employee

Hello,

Actually we migrate the kernels every year.

So we will wait for this issue to be completely solved in future Linux kernel and then we will use this kernel.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,150 次查看
MichaelChristian
Contributor I

This topic is now 6 years old. I am using BSP L4.1.15_2.0.0 which has the year 2038 problem. Has a current BSP addressed the 2038 problem yet, and if not what are the plans in this area?

0 项奖励
回复
3,396 次查看
b36401
NXP Employee
NXP Employee

Hello,

Actually we migrate the kernels every year.

So we will wait for this issue to be completely solved in future Linux kernel and then we will use this kernel.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复