Regarding drive strength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding drive strength

4,699 Views
surendrajadhav
Contributor IV

Hi,

We are working on ENET2 interface of i.MX6UL. We have observed one thing that when we keep drive strength enable value for ethetnet signals (except clock) to 240 ohm, ethernet communication work.

However if we make drive strength enable to 40 ohm, ethernet communication does not work.

Can you clarify that reducing drive strength enable value reduces drive strength of the pin and increasing drive strength enable value increases drive strength of the pin?

We thought that when we increasing value for 240 ohm, it reduces current as per ohms law and 40 ohm increase current value and thereby drive strength.

Please confirm.

Regards,

Surendra

Labels (1)
0 Kudos
Reply
3 Replies

4,447 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Board's signals trace impedance should match outputs and inputs impedance.

Please look at section 3 (i.MX 6UltraLite layout recommendations) of the

Hardware Development Guide.

https://www.nxp.com/docs/en/user-guide/IMX6ULHDG.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,448 Views
surendrajadhav
Contributor IV

Hi Yuri,

Thanks a lot for your reply.

However our concern is with drive strength and not with ODT(On Die Termination).

We are confused about drive strength that increasing resistor value (on chip strength resistance value between 34 ohm to 240 ohm) increases drive strength and reducing value reduces drive strength.

Regards,

Surendra

0 Kudos
Reply

4,448 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the drive strength is equivalent of output impedance.

Regards,

Yuri.

0 Kudos
Reply