Regarding Yocto and Linux versions of i.MX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding Yocto and Linux versions of i.MX

ソリューションへジャンプ
3,493件の閲覧回数
AnuDavis
Contributor I

When I came across different Yocto and Linux versions of i.MX, I got following doubts:

Question 1) What is F means in IMXLXRN v.LF5.4.3_1.0.0 ?

Question 2) what is its significance or difference compared to other releases, as I cannot see F in other version tags?

a) IMXLXRN v.L5.4.3_2.0.0

Date: 04/2020

Description: i.MX 5.4 Alpha release for i.MX 8M Plus and 8DXL EVK
boards.
b) IMXLXRN v.LF5.4.3_1.0.0

Date: 03/2020

Description: i.MX 5.4 Kernel and Yocto Project Upgrades.
c) IMXLXRN v.L4.19.35_1.1.0

Date: 10/2019

Description: i.MX 4.19 Kernel and Yocto Project Upgrades.

Please help me to understand.

0 件の賞賛
返信
1 解決策
3,449件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

LF stands for Linux Factory. LF should be a way to newer nomenclature for released BSP.

 

Regards

Harvey

元の投稿で解決策を見る

1 返信
3,450件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

LF stands for Linux Factory. LF should be a way to newer nomenclature for released BSP.

 

Regards

Harvey