Regarding QT5-example on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding QT5-example on iMX6

1,698 Views
umashankergupta
Contributor I

Hi Sir,

I am developing an application in qt and i want it to be deployed to my iMX6 .

I have created the application in my qt5 , build the project and the executable had been created and copy the executable on iMX6. But  when i try to execute the executable i am getting following errors.

root@iWave-G15M:/opt# export DISPLAY=:0
root@iWave-G15M:/opt#
root@iWave-G15M:/opt# ./Triangle
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
Unable to find an X11 visual which matches EGL config 5

and i'm also facing the same problem while running the inbuilt opengl example (hellogl2, cube etc.)

please can anyone help me out.

Regards,

Uma Shankar Gupta

0 Kudos
Reply
1 Reply

1,573 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Uma,

It may be useful to apply to QT experts.

Nevertheless, below is some link, which – hope – can help.

pkg/48553: Qt5 can't find compose files 

Regards

0 Kudos
Reply