Regarding 3D rendering on multiple screen using i.MX6Q processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding 3D rendering on multiple screen using i.MX6Q processor

1,740件の閲覧回数
VishalMore
Contributor I

Dear NXP team,

Could you please provide your inputs on below solution for stated problem?

Problem Statement: Is, 3D rendering scene possible on two screens with different resolutions simultaneously using an i.MX6Q processor?

Solution: 

VishalMore_0-1694610489040.png

Description:-
1. Create all necessary OpenGL Object required for rendering
2. OpenGL application will receive the data every 50ms
3. Create two different framebuffers (Backbuffers and frontbuffers) for two different Screens.
4. GPU will write 3D rendering Model data in Backbuffer-1 and Backbuffer-2.
4. Once, 3D rendering Model data is updated in both the Backbuffers, then swap the buffers to render the 3D Model on the screen at same time.

Please provide valuable inputs on the above solution.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,691件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

I do not think the MX6Q can do that especially the number 4, but you can select the i.MX8MQ for that task.

Regards

0 件の賞賛
返信

1,683件の閲覧回数
VishalMore
Contributor I

Thanks NXP team for reply.

Just for clarification, which one below steps 4 you are referring will have issue in i.MX6Q and if you can explain reason for same that will help to understand limitation

4. GPU will write 3D rendering Model data in Backbuffer-1 and Backbuffer-2.
4. Once, 3D rendering Model data is updated in both the Backbuffers, then swap the buffers to render the 3D Model on the screen at same time.

Thanks.

0 件の賞賛
返信