Reg: Touch Screen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reg: Touch Screen

14,176件の閲覧回数
vishvapathi
Contributor V

Hi All,

I am interested in interfacing Touch Screen with my EVB. I am getting Display in my screen, but not able to use Touch Screen.

Kindly advice how to enable and calibrate for touch screen.

Vishva

DaianeAngolini

ラベル(2)
34 返答(返信)

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Let´s start from the beginning:

What´s your board?

What´s your kernel?

What´s your rootfs maker?

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V

I am using I.MX 6Q SABRE SDB. Kernel - L3.0.35. LTIB

0 件の賞賛
返信

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I think it´s 2 step debug;

* Are your touchscreen driver working?

- try with "evtest" and see if you can get the touch events from kernel

* Are your touch calibrated?

- try Qt-embedded Touch screen problem on IMX53 (SABRE tablet)

Please, let me know

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V

Hi Daiane,

evtest /dev/input/event0                                
Input driver version is 1.0.1                                             
Input device ID: bus 0x0 vendor 0x0 product 0x0 version 0x0               
Input device name: "ads7846"                                              
Supported events:                                                         
  Event type 0 (Sync)                                                     
  Event type 1 (Key)                                                      
Event code 330 (Touch)                                                
  Event type 3 (Absolute)                                                 
Event code 0 (X)                                                      
  Value  0                                                        
  Min    0                                                        
  Max 4095                                                        
Event code 1 (Y)                                                      
  Value  0                                                        
  Min    0                                                        
  Max 4095                                                        
Event code 24 (Pressure)                                              
  Value  0                                                        
  Min    0                                                        
  Max    0                                                        

Testing ... (interrupt to exit)

0 件の賞賛
返信

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

and, when you tap your display you can see data coming?

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V

Nope... its just blank...

0 件の賞賛
返信

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

So, the problem is the driver

Do you know what LCD/LVDS panel you have?

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V

Bought it from embest technologies.. not sure abt make.....

0 件の賞賛
返信

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Do you have a picture?

Partnumber?

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V
0 件の賞賛
返信

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

is this connected as USB?

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V

No... Lvds..

0 件の賞賛
返信

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Have you changed your kernel command line?

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V

To wat???

0 件の賞賛
返信

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

ussualy I add

video=mxcfb1:dev=ldb,LDBXGA,if=RGB666



to the default LVDS pannel for imx6qsabresd

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V

Ya.. to set environment I did the same. M getting display, only touch is not working...

0 件の賞賛
返信

8,322件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

double check if the touchscreen driver is selected in menuconfig.

make sure to use the right one for your display

0 件の賞賛
返信

8,322件の閲覧回数
vishvapathi
Contributor V

Hi,

  I tried the same in MarS board also. I am getting only the display, touch is not working.:smileysad:

0 件の賞賛
返信

8,321件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Could you share what do you changed on your kernel configuration? (make menuconfig)

0 件の賞賛
返信

8,321件の閲覧回数
vishvapathi
Contributor V

I have selected ADS7846/TSC2046/AD7873 and AS(S)7843 based touch screens in device drivers selection. i am recompiling and trying it again..