Reg: Silex Wifi Module Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reg: Silex Wifi Module Driver

1,624件の閲覧回数
vishvapathi
Contributor V

Hi All,

I am trying to interface Wifi module as per the Application note. But getting error. Attached Commands and Responses for your reference. Kindly where i have gone wrong.

# cd /lib/firmware/ath6k/AR6003/hw2.1.1

# ln –s calData_SX-SDMAN.bin bdata.bin

Reposnse: ln: creating symbolic link `bdata.bin': File exists


Command: insmod ath6kl.ko

Response: insmod ath6kl.ko

mmc1: queuing unknown CIS tuple 0x01 (3 bytes)

mmc1: queuing unknown CIS tuple 0x1a (5 bytes)

mmc1: queuing unknown CIS tuple 0x1b (8 bytes)

mmc1: queuing unknown CIS tuple 0x14 (0 bytes)

ath6kl: Failed to get patch file ath6k/AR6003/hw2.1.1/data.patch.bin: -2

ath6kl: Failed to init ath6kl core

ath6kl_sdio: probe of mmc1:0001:1 failed with error -2

ラベル(2)
0 件の賞賛
返信
0 返答(返信)