Reference schematic of i.MX6UL and PF3000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reference schematic of i.MX6UL and PF3000

3,500 次查看
ko-hey
Senior Contributor II

Hi all

Is there a reference schematic that it use both i.MX6UL and PF3000 ?

Ko-hey

标签 (2)
标记 (2)
0 项奖励
回复
6 回复数

2,052 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   I am afraid the only available PF3000 design for i.MX6 series is provided in app note

"Powering an i.MX 6SL Based System Using the PF3000 PMIC".

http://cache.freescale.com/files/analog/doc/app_note/AN5113.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,052 次查看
ko-hey
Senior Contributor II

Hi Yuri

Thank you for reply.

I understand a current situation.

Is there any plan to release the PF3000 design for i.MX6UL ?

Ko-hey

0 项奖励
回复

2,052 次查看
fabio_estevam
NXP Employee
NXP Employee

Yes, there is a board called imx6ul-9x9-evk that uses the  pfuze3000 PMIC.

You can refer its device tree at:

linux-2.6-imx.git - Freescale i.MX Linux Tree

Regards,

Fabio Estevam

0 项奖励
回复

2,052 次查看
satoshishimoda
Senior Contributor I

Hi Fabio,

Can I get the schematics of imx6ul-9x9-evk now?

Or only device tree is released?

Best Regards,

Satoshi Shimoda

0 项奖励
回复

2,052 次查看
Yuri
NXP Employee
NXP Employee

Hi,

I do not have any information about plans to "release the PF3000 design for i.MX6UL", :smileysad:

~Yuri.

0 项奖励
回复

2,052 次查看
ko-hey
Senior Contributor II

OK, Thanks.

Ko-hey

0 项奖励
回复