Redundant boot build Instructions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Redundant boot build Instructions

2,812 次查看
lockit282
Contributor III

1. Is there documentation for building the redundant bootloader (secondary boot) without fastboot for the imx8mm in an android environment?
2. Can the Secondary bootloader be used in a non-secure environment -- manually set the PErsist bit)?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

2,500 次查看
lockit282
Contributor III

My question is -- what is the best way to get the secondary image table onto the emmc per the documentation in the imx8mm security manual -- and this app note : i.MX 8MQ - ROM Redundant Boot for expansion device 
1. When I look at the fastboot code to flash u-boot the start offset on the emmc is 0x42

2. I am using an Android environment w/Secure boot

Question 1: How to program the secondary image table on the imx8mm eMMC per Chapter 6 of the Imx8mm Security manual?

Question 2: The secondary bootloader -- can it be a copy of the primary?

0 项奖励
回复

2,500 次查看
lockit282
Contributor III

This for flashing onto emmc

0 项奖励
回复