Redhat Linux support for i.MX6Q Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Redhat Linux support for i.MX6Q Processor

2,704 Views
anandmeharwade
Contributor II

Hi All,

Hope your are doing good.

In one of our application we need to have the Redhat linux support. Could you please let us know the availability of resources and support from freescale in this regard.

Looking forward to hear from you soon.

Regards

Anand M

Labels (2)
0 Kudos
Reply
3 Replies

2,446 Views
jamesbone
NXP TechSupport
NXP TechSupport

Basically Freescale provide a Linux BSP , which can be used together with the root file system of Red Hat something similar for what we have with Ubuntu. But I apologize that we do not have something else to show you. Regarding the support you can always use our Engineering Services it is not for free, here is a presentation of what we offer:

http://cache.freescale.com/files/training/doc/ftf/2014/FTF-SDS-F0251.pdf

http://www.freescale.com/files/training/doc/dwf/DWF13_AMF_ENT_T1024.pdf


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,446 Views
RobertA
Contributor I

Hello Jaime,

Does this mean freescale has a Red Hat root file system for the IMXQ6, similar to Ubuntu? If so can you send me a link for it.

Best Regards,

Alex

0 Kudos
Reply

2,446 Views
jamesbone
NXP TechSupport
NXP TechSupport

Freescale only have Ubuntu Root File System.

0 Kudos
Reply