Recovery doesn't have some functions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recovery doesn't have some functions

ソリューションへジャンプ
2,558件の閲覧回数
lqll
Contributor III

Hi

My environment is i.MX6Q and Android4.4.2 1.0.0-rc3

I want to modify update.zip to support update uboot,and I follow Android_Frequently_Asked_Questions.pdf 's section How do I customize the reference OTA application

I added this command to the end of updater-script

# Write u-boot to 1K position.

# u-boot binary should be a no padding uboot!

# For eMMC(iNand) device, needs to unlock boot partition.

ui_print("writting u-boot...");

package_extract_file("files/u-boot-6q.bin", "/tmp/u-boot-no-padding.bin");

sysfs_file_write("class/mmc_host/mmc0/mmc0:0001/boot_config", "1");

simple_dd("/tmp/u-boot-no-padding.bin", "/dev/block/mmcblk0", 1024);

sysfs_file_write("class/mmc_host/mmc0/mmc0:0001/boot_config", "8");

show_progress(0.1, 5);

When I enter recovery mode,I failed and get this log:

Finding update package...

I:Update location: /cache/update.zip

Opening update package...

I:read key e=3 hash=20

I:1 key(s) loaded from /res/keys

Verifying update package...

I:comment is 1746 bytes; signature 1728 bytes from end

I:whole-file signature verified against key 0

I:verify_file returned 0

Installing update...

line 89 col 67: unknown function "sysfs_file_write"

line 90 col 68: unknown function "simple_dd"

line 91 col 67: unknown function "sysfs_file_write"

3 parse errors

E:Error in /cache/update.zip

(Status 6)

Installation aborted.

It said I didn't have some functions.Then I check what functions do I have in recovery,I get this:

./edify/expr.c:    RegisterFunction("ifelse", IfElseFn);

./edify/expr.c:    RegisterFunction("abort", AbortFn);

./edify/expr.c:    RegisterFunction("assert", AssertFn);

./edify/expr.c:    RegisterFunction("concat", ConcatFn);

./edify/expr.c:    RegisterFunction("is_substring", SubstringFn);

./edify/expr.c:    RegisterFunction("stdout", StdoutFn);

./edify/expr.c:    RegisterFunction("sleep", SleepFn);

./edify/expr.c:    RegisterFunction("less_than_int", LessThanIntFn);

./edify/expr.c:    RegisterFunction("greater_than_int", GreaterThanIntFn);

./updater/install.c:    RegisterFunction("mount", MountFn);

./updater/install.c:    RegisterFunction("is_mounted", IsMountedFn);

./updater/install.c:    RegisterFunction("unmount", UnmountFn);

./updater/install.c:    RegisterFunction("format", FormatFn);

./updater/install.c:    RegisterFunction("show_progress", ShowProgressFn);

./updater/install.c:    RegisterFunction("set_progress", SetProgressFn);

./updater/install.c:    RegisterFunction("delete", DeleteFn);

./updater/install.c:    RegisterFunction("delete_recursive", DeleteFn);

./updater/install.c:    RegisterFunction("package_extract_dir", PackageExtractDirFn);

./updater/install.c:    RegisterFunction("package_extract_file", PackageExtractFileFn);

./updater/install.c:    RegisterFunction("symlink", SymlinkFn);

./updater/install.c:    RegisterFunction("set_perm", SetPermFn);

./updater/install.c:    RegisterFunction("set_perm_recursive", SetPermFn);

./updater/install.c:    RegisterFunction("set_metadata", SetMetadataFn);

./updater/install.c:    RegisterFunction("set_metadata_recursive", SetMetadataFn);

./updater/install.c:    RegisterFunction("getprop", GetPropFn);

./updater/install.c:    RegisterFunction("file_getprop", FileGetPropFn);

./updater/install.c:    RegisterFunction("write_raw_image", WriteRawImageFn);

./updater/install.c:    RegisterFunction("apply_patch", ApplyPatchFn);

./updater/install.c:    RegisterFunction("apply_patch_check", ApplyPatchCheckFn);

./updater/install.c:    RegisterFunction("apply_patch_space", ApplyPatchSpaceFn);

./updater/install.c:    RegisterFunction("read_file", ReadFileFn);

./updater/install.c:    RegisterFunction("sha1_check", Sha1CheckFn);

./updater/install.c:    RegisterFunction("rename", RenameFn);

./updater/install.c:    RegisterFunction("wipe_cache", WipeCacheFn);

./updater/install.c:    RegisterFunction("ui_print", UIPrintFn);

./updater/install.c:    RegisterFunction("run_program", RunProgramFn);

and there are no sysfs_file_write and simple_dd,then I check the recovery's git log,I get this:

commit 4f14fa3dbed753ed474afc953e759934e48b2323

Author: guoyin.chen <guoyin.chen@freescale.com>

Date:   Fri Aug 23 17:27:30 2013 +0800

    ENGR00275477 Recovey: Mess code when enter recovery mode

   

    Init the text array to make sure default text is null

   

    Signed-off-by: guoyin.chen <guoyin.chen@freescale.com>

Do I have the wrong version?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,666件の閲覧回数
gary_bisson
Senior Contributor III
2 返答(返信)
1,667件の閲覧回数
gary_bisson
Senior Contributor III
1,666件の閲覧回数
lqll
Contributor III

Hi Gary

It works,thank you very much!

Qiulong Li

0 件の賞賛
返信