Recommendations for MX28 development.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommendations for MX28 development.

ソリューションへジャンプ
4,449件の閲覧回数
RandyGraham
Contributor IV

Hello,

I am new to the i.mx family and am looking for a few general recommendations so I get started off in the right direction.

So far I have built linux 2.6.35 using LTIB and have it running on my M28 EVK.

My first question is, should I stick with LTIB or are there better BSP-build alternatives for i.mx28 (e.g. ptxdist, YOCTO), assuming I'll need to move to a 3.x kernel at some point ?

Next question is, I am developing an app for my MX28 EVK board that needs to talk to a SPI device on SSP2 and could use some pointers on how to set up the board file and spidev. Also, how is SPI support in the 3.x kernels?

Thanks for any help.

ラベル(2)
1 解決策
3,859件の閲覧回数
RandyGraham
Contributor IV

I am successfully using buildroot to build the 3.7-rc1 kernel and rootfs for my m28evk and will stick with that moving forward.

-Randy

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,860件の閲覧回数
RandyGraham
Contributor IV

I am successfully using buildroot to build the 3.7-rc1 kernel and rootfs for my m28evk and will stick with that moving forward.

-Randy

0 件の賞賛
返信
3,859件の閲覧回数
imxcommunitysco
Senior Contributor II

Randy, if your question had been answered, please mark the reply from the person who provide correct answers as 'Correct Answer'. So that we can close the discussion.

0 件の賞賛
返信
3,859件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You also can read the BSP Reference Manual for more details. Chapter 21 is talking about the SPI Bus driver.

0 件の賞賛
返信
3,859件の閲覧回数
YS
Contributor IV

My previous article will some help for spidev configuration on iMX28EVK Linux.

SPI: SPIDEV interface question

Note that iMX28 SPI base clock is fixed to 120MHz and SPI clock is 1/n (n >= 2) of the base clock.

If this is inconvenient, you may try to change base clock at drivers/spi/spi_mxs.c at

static int __init mxs_spi_probe(struct platform_device *dev)

    .

    .

    .

    clk_set_rate(ss->clk, 120 * 1000 * 1000)

For spidev usage, there is good description in Linux Kernel document linux-2.6.35.3/Documentation/spi/.

3,859件の閲覧回数
RandyGraham
Contributor IV

Thanks Yuji, this is helpful !

0 件の賞賛
返信