Recommendation needed on how to use USB1 for DDR training (USB_OTG1) and SCH-29918

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommendation needed on how to use USB1 for DDR training (USB_OTG1) and SCH-29918

ソリューションへジャンプ
190件の閲覧回数
BF2025
Contributor II

We are developing  a custom processor card using the IMX8 QuadPlus processor and using the MEK schematic as a reference.


We would like to allow Serial Boot so we can do DDR4 training via the provided scripts.

We have no use for USB-C and are planning to use the USB 2.0 OTG1  to boot for use in  this script - we have no other usage for this USB.

I cannot find the reference schematic for the Base Board (which has the USB 2.0 connector) , its reference MCIMX8-8X-BB (or SCH-29918) does not give any results on Schematic Design files.

 

I am not that familiar with USB - so advice on how to power it and how to switch Modes using the ID pin are appreciated.

Also if we could get the Base Board schematic as the MEK circuit only shows the CPU card side of the USB interface.

So far I understand that the processor should enable the power to the USB bus but I am not clear on the finer details.

Many thanks 

Boris.

 

0 件の賞賛
返信
1 解決策
169件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I can attach it to you , please check it:

 

元の投稿で解決策を見る

3 返答(返信)
142件の閲覧回数
BF2025
Contributor II

Many thanks appreciate the reply !

134件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome~~

0 件の賞賛
返信
170件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I can attach it to you , please check it: