Receiving unknown event in imu sensor hal with imx6 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Receiving unknown event in imu sensor hal with imx6 board

1,300件の閲覧回数
shilesh_babu
Contributor II

Dear All,

I am getting below error while integrated sensor hal with imx6, can any one help me out.

when i do logcat below message are coming.... 
01-01 01:43:29.319 286 468 E Sensors : GyroSensor: unknown event (type=3, code=2)
01-01 01:43:29.321 286 286 E Sensors : AccelSensor: unknown event type (type = 3, code = 0)
01-01 01:43:29.321 286 286 E Sensors : AccelSensor: unknown event type (type = 3, code = 1)
01-01 01:43:29.321 286 286 E Sensors : AccelSensor: unknown event type (type = 3, code = 2)
01-01 01:43:29.331 286 468 E Sensors : MagnSensor: unknown event (type = 3, code = 0)
01-01 01:43:29.331 286 468 E Sensors : MagnSensor: unknown event (type = 3, code = 1)
01-01 01:43:29.331 286 468 E Sensors : MagnSensor: unknown event (type = 3, code = 2)
01-01 01:43:29.335 286 286 E Sensors : GyroSensor: unknown event (type=3, code=0)
01-01 01:43:29.335 286 286 E Sensors : GyroSensor: unknown event (type=3, code=1)
01-01 01:43:29.335 286 286 E Sensors : GyroSensor: unknown event (type=3, code=2)
01-01 01:43:29.337 286 468 E Sensors : AccelSensor: unknown event type (type = 3, code = 0)
01-01 01:43:29.337 286 468 E Sensors : AccelSensor: unknown event type (type = 3, code = 1)
01-01 01:43:29.337 286 468 E Sensors : AccelSensor: unknown event type (type = 3, code = 2)
01-01 01:43:29.347 286 286 E Sensors : MagnSensor: unknown event (type = 3, code = 0)
01-01 01:43:29.347 286 286 E Sensors : MagnSensor: unknown event (type = 3, code = 1)
01-01 01:43:29.347 286 286 E Sensors : MagnSensor: unknown event (type = 3, code = 2)
01-01 01:43:29.351 286 468 E Sensors : GyroSensor: unknown event (type=3, code=0)
01-01 01:43:29.351 286 468 E Sensors : GyroSensor: unknown event (type=3, code=1)
01-01 01:43:29.351 286 468 E Sensors : GyroSensor: unknown event (type=3, code=2)
01-01 01:43:29.354 286 286 E Sensors : AccelSensor: unknown event type (type = 3, code = 0)
 

when i do getevent below logs are coming ....

/dev/input/event0: 0003 0000 ffffd120
/dev/input/event0: 0003 0001 ffffb80c
/dev/input/event0: 0003 0002 fff0ce50
/dev/input/event0: 0000 0000 00000000
/dev/input/event2: 0003 0000 00021dcc
/dev/input/event2: 0003 0001 00002c7c
/dev/input/event2: 0003 0002 00019a0e
/dev/input/event2: 0000 0000 00000000
/dev/input/event1: 0003 0000 002cba32
/dev/input/event1: 0003 0001 00294186
/dev/input/event1: 0003 0002 fff0a556
/dev/input/event1: 0000 0000 00000000

When i do cat /dev/input/event0 or cat /dev/input/event1 or cat /dev/input/event2 receiving below logs on console.

cat /dev/input/event0 � d����
��� ��� ���� ���� � ���� ����� � 8���� � ����� ����� ����� � ����� t���� �����
���� �� d���� ����� � % ���� ����� p���� % h���� % � e ����� e X���� e ���� e � �
d (���� � 8���� � �
����� d

Can anyone let me know, what can we the rootcause for this Error. it is bit urgent for me your help will be highly appreciated.

Thanks in advance.

ラベル(6)
0 件の賞賛
返信
1 返信

1,231件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信