Reboot not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reboot not working

2,373 Views
_andev_
Contributor II

Hi,

I have a custom board based on imx6 dual. I'm updating to BSP 4.9.11 and I have a problem with the reboot. I'm using sysvinit and the command:

#  shutdown.sysvinit -r 0

does a shutdown but the board don't reboot. The same step in my current BSP 3.14.52 based, is working ok. Something in the kernel to check?

Thanks!

Jorge

0 Kudos
Reply
4 Replies

2,151 Views
Yuri
NXP Employee
NXP Employee

Hello,

 It is highly recommended to remove power (voltage source) to all components on the board in the  
event of a processor reset. This avoids having to determine if a component critical to rebooting the  
processor is in the necessary state to support a reboot.

  I.MX validation boards and NXP sponsored third-party boards have all been designed to remove
power (Voltage source) to all components on the board in the event of a processor reset.

  So, the POR may be recommended for reboot.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,151 Views
_andev_
Contributor II

Hi Yuri!

Well, I think the power is ok because the same hardware with an older kernel version is rebooting ok but with the newer one it isn't. Is there any way to force a reset? What do you mean with "the POR may be recommended for reboot" ?

Thanks!

Jorge

0 Kudos
Reply

2,151 Views
Yuri
NXP Employee
NXP Employee

Hello,

   The issue, when i.MX device reset is applied for system reboot, but reboot does not finish 
successfully, is from kind of application / situation dependent one and not obviously has 100%

probability to occur.   You may look at i.MX6 reference designs, where system reset / reboot

is implemented via WDOG, which in its turn asserts system POR via PMIC.

Regards,

Yuri.

0 Kudos
Reply

2,151 Views
_andev_
Contributor II

I've checked the sysvinit version in both BSP and it's the same version 2.88dsf-r14. Then I guess it's the kernel fault. It's able to shutdown the device but not to reboot it.

0 Kudos
Reply