Reassign Controller Area Network (CAN) interfaces to UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reassign Controller Area Network (CAN) interfaces to UART

879 次查看
shailendrakarod
Contributor I

I want to use the two CAN (DB-9) interfaces on i.mx 6solox development board as UARTs. Is this possible? If yes then can I use these UARTs from M4?

标签 (1)
0 项奖励
回复
1 回复

819 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shailendra

please check

Reuse CAN interface for UART communication 

both cores can access modules if RDC is configured properly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复