Reassign Controller Area Network (CAN) interfaces to UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reassign Controller Area Network (CAN) interfaces to UART

894 Views
shailendrakarod
Contributor I

I want to use the two CAN (DB-9) interfaces on i.mx 6solox development board as UARTs. Is this possible? If yes then can I use these UARTs from M4?

Labels (1)
0 Kudos
Reply
1 Reply

834 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shailendra

please check

Reuse CAN interface for UART communication 

both cores can access modules if RDC is configured properly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply