Reassign Controller Area Network (CAN) interfaces to UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reassign Controller Area Network (CAN) interfaces to UART

880件の閲覧回数
shailendrakarod
Contributor I

I want to use the two CAN (DB-9) interfaces on i.mx 6solox development board as UARTs. Is this possible? If yes then can I use these UARTs from M4?

ラベル(1)
0 件の賞賛
返信
1 返信

820件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shailendra

please check

Reuse CAN interface for UART communication 

both cores can access modules if RDC is configured properly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信