Reason for Difference in Gigabit Performance on Ubuntu vs. Android JB4.3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reason for Difference in Gigabit Performance on Ubuntu vs. Android JB4.3?

1,712件の閲覧回数
carsongreen
Contributor I

TCP performance measured using iperf on the sabresd device using the built in gigabit with Android JB4.3 is around 320 Mbps while on Ubuntu is around 450 Mbps. What is the bottleneck in the Android network? Is there anyway to potentially optimize the Android build to better match the performance of using Ubuntu? What expectation can I have for network performance with a network adapter connected over PCIe. I have measured PCIe bus speeds to get at least as high as 1.4 Gbps, however I am concerned that the Android network stack running on the sabresd device may not be able to handle data rates at those speeds.

I have seen some other post discussing poor network performance in Android such as About Gigabit Ethernet performance gap between Android&Linux and http://boundarydevices.com/i-mx6-ethernet/ but in these post, test show lots of dropped packets and I am getting very little dropped packets. I have also tested reducing tcp_mem, tcp_rmem and tcp_wmem in Ubuntu to what it is in Android and this had very little impact on performance so I don't think lack of available tcp memory is the problem.

Thanks,

Carson

ラベル(3)
0 件の賞賛
返信
1 返信

1,523件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Carson,

I think link below answers your question.

In general obviously different OS may have different performance

due to different memory layout, driver structure and associated with

it bus loading.

About Gigabit Ethernet performance gap between Android&Linux

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信