Read LICELL Voltage in Software (Linux) from MMPF0200

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Read LICELL Voltage in Software (Linux) from MMPF0200

ソリューションへジャンプ
2,896件の閲覧回数
neuro
Contributor III

Hello,

I am currently running a system with an i.MX6 Solo X and a PF 200 power manager component. I am also running Linux.

I want to read the current voltage of the coin cell from the power manager device (LICELL pin).

I've been reading http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf?fasp=1&WT_TYPE=Data%20Sheets&WT_... 

but no luck. I realize there is the i2c control for the coin cell however I don't want to set the voltage but only read the current voltage coming out of the battery via the power manager.

If there is a way to read on linux via sysfs that would be best. I know of the regulator devices in /sys/class/regulators but I'm not sure which one would be the for the external lithium ion battery (LICELL).

Thank you

0 件の賞賛
返信
1 解決策
2,784件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, that is impossible. You can only set an output voltage. Probably, that is because it needs to be done by a tensor divisor. This type of topology will drop out your output your voltage and it could drain your battery cell.

Best regards,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,785件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, that is impossible. You can only set an output voltage. Probably, that is because it needs to be done by a tensor divisor. This type of topology will drop out your output your voltage and it could drain your battery cell.

Best regards,

Diego.

0 件の賞賛
返信
2,784件の閲覧回数
neuro
Contributor III

Thank you.

After reading your comment, this makes sense. If you want to read the battery you are draining it with that type of circuitry.

0 件の賞賛
返信