Re-programming of the PMIC in the SCM SoloX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re-programming of the PMIC in the SCM SoloX

782件の閲覧回数
erezamir
Contributor II

Hello,

We have the EVB of the SCM-I.mx6SX.
In order to boot from the serial downloader (OTG USB) there is a need for 5V supply. We do not want to use an external supply of 5V, instead use the internal SWBST of the PMIC.
The PMIC is pre-configured with SWBST_SEQ set to 0 so the SWBST does not turn on by default.
We re-programmed the PMICs OTP fuses to enable the SWBST to turn on, and SWBST turns on as expected.
We read the OTP_ECCI bit and it indicates an error (OTP_ECCI=1) .
The appnote (AN4536) specifies that if the OTP_ECCI bit is 1 - the part should be rejected.

Can you please clarify what should be done in this situation?
Is there any guidlines how to re-program a PMIC which was pre-programmed?

Thanks,

ラベル(3)
0 件の賞賛
返信
0 返答(返信)