Re: iMX6UL-EVK: How do I use MFG-TOOL to boot from QSPI Nor Flash?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: iMX6UL-EVK: How do I use MFG-TOOL to boot from QSPI Nor Flash?

1,118 次查看
nitigupta
Contributor I

Hello All,

I am also trying to boot Linux from QSPI and also tried MFG tool to do the same but MFG tool script allows to copy only u-boot to QSPI as well as QSPI header. I want to burn zImage, device tree & root file system also on QSPI but failed to understand how to do partition of QSPI flash.
Is there any tutorial available for the same. Any help is appreciated.

Thanks,
Niti

0 项奖励
回复
1 回复

869 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Additionally it may be required to configure  U-boot environment to boot properly kernel.

Please look at section 4.7.4 (Running the Linux OS image from QuadSPI) in “i.MX_Linux_User's_Guide.pdf”.

 

< http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... >

  Also, please look at the following :

https://community.nxp.com/message/491138 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复