Re: Which ECC i.MX6 ROM code uses?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Re: Which ECC i.MX6 ROM code uses?

跳至解决方案
2,241 次查看
abdulrasheed
Contributor I

YuriMuhin_ng‌ I used your attached BCH_enco.c and found that it generates incorrect code for some data blocks.
is there any updated version of this file is available?
This file generated incorrect/different ECC for program_image as compare to ECC generated by kobs-ng utility for NAND.

0 项奖励
回复
1 解答
2,125 次查看
b36401
NXP Employee
NXP Employee

The algorithm Yuri attached is one used on i.MX6 processors.
And the same BCH ECC is used on i.MX7 and i.MX8M processors as well.
Please make sure that you set right parameters for encoding algorithm.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,125 次查看
b36401
NXP Employee
NXP Employee

Additionally to doublecheck if it is right algorithm please create a technical case:
https://community.nxp.com/thread/381898
I will attach the file.

0 项奖励
回复
2,126 次查看
b36401
NXP Employee
NXP Employee

The algorithm Yuri attached is one used on i.MX6 processors.
And the same BCH ECC is used on i.MX7 and i.MX8M processors as well.
Please make sure that you set right parameters for encoding algorithm.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复